Introducing the Grundfos SCALA2

24/05/2016

Grundfos has long been regarded for their high quality and reliable pumps. The Grundfos SCALA2 takes design innovation, comfort and simplicity to the next level and is set to be a game changer in domestic boosting.

The new SCALA2 is a robust, fully integrated, self-priming pump suitable for use from both above and below ground water sources. The compact system features a pump, motor, tank, sensor, drive and non-return valve in one compact unit that is quick and easy to install.

The SCALA2 is an energy efficient pump featuring an integrated speed controller that ensures constant water pressure regardless of variations in demand or inlet pressure.


The variable speed controller also matches the power consumption with the required water output, which also helps to conserve energy and reduce your energy bills.

To protect the pump and help ensure a long life, the SCALA2 includes a range of protective features. Dry run protection automatically stops operation when the  water source runs out, to help prevent damage, and the anti-cycling feature detects any unnatural cycling and alerts the user via the protection indicator on the control panel.

For those living in areas of poor power supply or those that are sometime affected by power outages, the SCALA2 can also be run on a generator, due to its ability to be able to handle varying voltages.  

Another unique benefit of the SCALA2 is its quiet operation, thanks to the permanent magnet motor and water cooling technology. The high efficiency motor is significantly quieter than traditional speed-controlled motors and the SCALA2 is cooled by the water it pumps, eliminating the need for a noisy fan. This makes the SCALA2 one of the quietest domestic boosting pumps currently available on the market.

And for ease of selection, the SCALA2 suits most domestic pressure boosting applications and is capable of supplying water for small single level homes up to larger multi-storey homes.

Speak to your local Authorised Grundfos Dealer today or visit www.grundfos.com.au/SCALA2 for more information.


    Facebook Twitter LinkedIn